AXIS#.IL.COMPTABLE.MAX
Description
AXIS#.IL
"Instruction list"
This is a low-level language and resembles assembly.COMPTABLE.MAX sets the cogging compensation/torque
Torque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist compensation table index maximum. The table ends at the defined maximum axis position.
When AXIS#.PL.FB is equal to AXIS#.IL.COMPTABLE.MAX, the output of the table will be equal to the last table entry.
-
-
The units of AXIS#.IL.COMPTABLE.MAX is determined by the value of AXIS#.UNIT.PROTARY or AXIS#.UNIT.PLINEAR.
Example
To set the of the table to 360 degrees, the user would enter:
-->AXIS1.IL.COMPTABLE.MAX 360
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-07-03-000 |
General Information
|
Type |
Read/Write |
|
Units |
Rotary: counts, rad, deg, custom units, 16-bit counts Linear: counts, mm, µm, custom units, 16-bit counts See Position Units for details. |
|
Range |
Depends on units. See Position Range for details. |
|
Default Value |
360.0 Degrees |
|
Data Type |
Float |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.IL.COMPTABLE.MAX | 0x500A | 0x1A | UINT | 1:1 | - | RW | False |
| AXIS2.IL.COMPTABLE.MAX | 0x510A | 0x1A | UINT | 1:1 | - | RW | False |